Publication on SFTP Server
Presentation
Panel Server provides a connection to an SFTP server.
When data sampling and publication to SFTP are activated, the sampled data of devices is published to the SFTP server in json or csv files. A maximum of one month of data (Entry or Universal) or three months of data (Advanced) is published to the SFTP server. If data sampling was activated before this period, older data is not published.
Alarms are managed as follows when SFTP publication is active:
-
Alarms can be monitored and displayed in Panel Server webpages.
-
Alarms are not published in the CSV or JSON files.
-
Alarms can be enabled for email notification.
When SFTP publication is active, data publication on cloud services or HTTPS is not available.
Availability
This function is available on Panel Server Entry, Universal, and Advanced.
Setting the Parameters
Publishing function is set on the Panel Server webpages:
-
For Panel Server Entry and Universal at .
-
For Panel Server Advanced at
Fill in the Connection information and Publication settings described in the following tables.
SFTP Publication Settings (Panel Server Entry and Universal)
The following table describes the settings.
|
Parameter |
Settings |
Description |
|---|---|---|
|
Connection information |
Server |
The host name of the SFTP server can be defined as the IP address
value or as, for example, |
|
Port |
Used to define the SFTP server TCP port. It is usually set to 22. |
|
|
Path |
Used to enter the path to use on the SFTP server for data publishing.
For example, if |
|
|
User ID |
Used to enter the SFTP user account name for the user account on the target SFTP server. |
|
|
Authentication method |
Used to select the authentication method to use when connecting to the SFTP server:
|
|
|
Password |
Used to type the password for SFTP server access. |
|
|
Import key file |
Button used to upload to Panel Server a file containing the encrypted password to use to connect to the SFTP server. Displayed when authentication method is by key. |
|
|
Test connection |
Button used to test connection to the SFTP server. |
|
|
Publication settings |
Publication format |
Used to select the exported file format:
|
|
Publication period |
Used to select the publication frequency to the SFTP server (default setting: 10 min). NOTE: The publication period is calculated from
the end of one publication to the start of the next. The time needed
for a publication varies depending on the quantity of data to be analyzed
and published.
|
|
|
Start |
Button used to launch data publication to the SFTP server. |
SFTP Publication Settings (Panel Server Advanced)
The following table describes the settings.
|
Parameter |
Settings |
Description |
|---|---|---|
|
Connection information |
Server |
The host name of the SFTP server can be defined as the IP address
value or as, for example, |
|
Port |
Used to define the SFTP server TCP port. It is usually set to 22. |
|
|
Path |
Used to enter the path to use on the SFTP server for data publishing.
For example, if |
|
|
User ID |
Used to enter the SFTP user account name for the user account on the target SFTP server. |
|
|
Authentication method |
Used to select the authentication method to use when connecting to the SFTP server:
|
|
|
Password |
Used to type the password for SFTP server access. |
|
|
Import key file |
Button used to upload to Panel Server a file containing the encrypted password to use to connect to the SFTP server. Displayed when authentication method is by key. |
|
|
Test connection |
Button used to test connection to the SFTP server. |
|
|
Publication settings |
Publication format |
Used to select the exported file format:
|
|
Publication period |
Used to select the publication frequency to the SFTP server (default setting: 10 min). NOTE: The publication period is calculated from
the end of one publication to the start of the next. The time needed
for a publication varies depending on the quantity of data to be analyzed
and published.
|
|
|
Include previously historized data toggle switch |
Used to include all data for past three months, or from the beginning of data sampling if less than three months. |
|
|
Start |
Button used to launch data publication to the SFTP server. Refer to Date and Content of the First Data Publication. |
Date and Content of First Data Publication (Panel Server Advanced)
The date and time of the first publication depends on the publication period set, as indicated in the following table.
| Publication period | First publication date and time and start of data collection |
|---|---|
|
Weekly |
00:00 on first Thursday following publication launch |
|
Daily |
00:00 following publication launch |
|
12h |
00:00 following publication launch |
|
4h |
At the next full hour (for example, launch publication at 10:47, publication starts at 11:00) |
|
3h |
At the next full hour (for example, launch publication at 10:47, publication starts at 11:00) |
|
2h |
At the next full hour (for example, launch publication at 10:47, publication starts at 11:00) |
|
1h |
At the next full hour (for example, launch publication at 10:47, publication starts at 11:00) |
|
10 min |
At the next interval of 10 minutes (for example, 10:10, 10:20, 10:30 etc) |
When the Include previously historized data toggle switch is selected, the first publication will contain all the data from the past three months, or from the beginning of data sampling if less than three months.
Connecting to SFTP Server
To connect the Panel Server to an SFTP server:
-
On the SFTP server, configure a connection for the publication of data from the Panel Server.
-
In the Panel Server webpage , click HTTP proxy or HTTPS proxy and enter the required information.
-
In the webpage, select the Publication method as follows:
-
For Panel Server Entry and Universal select .
-
For Panel Server Advanced select SFTP & Email for alarms
By default, SFTP data publications (CSV or JSON file format) are stored at the top of the hierarchical file tree of the SFTP server. If you customize the file path for the data storage, make sure that the path is created and validated on the SFTP server. For more information, refer to the user guide of your SFTP server.
-
-
To connect to the SFTP server, enter the user ID and password or user ID and SSH key in PEM (Privacy Enhanced Mail) format in the Connection information section. Save your settings by clicking the icon at bottom right of the screen and selecting Save.
-
Click Test connection. The list of SSH key exchanges and ciphers supported by the Panel Server is available in Appendix E.
When using SSH key authentication, the key must be provided in PEM format (default setting when relying on OpenSSH version less than 7.8).
NOTE: If it is the first time the Panel Server connects to this SFTP server, a message appears and requests that you confirm the authenticity of the SFTP server. -
Once the test is performed, the Panel Server webpage displays information:
-
In case of success, a file has been successfully uploaded on the SFTP server.
-
In case of dysfunction, check the SFTP server parameters, user credentials, and write access privileges on the SFTP server.
-
-
To publish data, set Publication settings and click Start.
Result: The sampled data of devices, related to the selected sampling period, is published to SFTP, in CSV file format or JSON format.
-
If you update the SFTP server, the SFTP server fingerprint changes. In this case, click Test connection to allow you to connect to the SFTP server again.
Disconnecting from Publishing Services
To disconnect Panel Server from the SFTP server, click Stop.
Disconnecting from the service allows you to connect to another publishing service.