DOCA0172EN-20

Wi-Fi Communication

Presentation

The EcoStruxure Panel Server supports the following Wi-Fi functions:

  • Wi-Fi infrastructure, that is, the Panel Server can connect to a Wi-Fi router (access point). For more information, refer to Wi-Fi Infrastructure.

  • Wi-Fi access point, that is, Panel Server can serve as a Wi-Fi router (access point) to which you can connect a smartphone or a PC. For more information, refer to Wi-Fi Access Point.

Availability

This function is available on Panel Server Entry, Universal (except Wired by Design models), and Advanced.

Setting the Parameters

Wi-Fi activation is enabled and disabled on the Panel Server webpages (disabled by default). Proceed as follows:

  1. Access the Panel Server webpages (see detailed topic).

  2. Enable and disable the Wi-Fi function on the webpage Settings > Network communication > Wi-Fi infrastructure > General settings > Wi-Fi activation.

NOTE: Wi-Fi activation is enabled automatically when the multifunction button on the front face of the Panel Server is pressed during commissioning of the Panel Server through EcoStruxure Energy Hub Essential (part of EcoStruxure Building Activate).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.