DOCA0172EN-20

Appendix H: Contextualization Data

Presentation

Contextualization data is assigned to devices during commissioning. It provides information about the context and use of the devices within the Panel Server system. The following types of contextualization data can be assigned:

  • Commodity

  • Usage

  • Zone

Commodity List

The following list indicates the commodities available to be assigned to devices and to use for filtering data on the Panel Server webpages:

  • Air

  • Electricity

  • Environment

  • Fuel Oil

  • Gas

  • Other

  • Steam

  • Water

Usage List

The following list indicates the usages available to be assigned to devices and to use for filtering data on the Panel Server webpages:

  • Air conditioning

  • Compressed air

  • Computer

  • Cooking

  • Cooling

  • Domestic hot water

  • Electrical vehicle charging station

  • Elevator

  • Emergency lighting

  • Food refrigeration

  • Genset

  • Heating

  • Heating & Air conditioning

  • Hot sanitary water

  • HVAC

  • IT

  • Lighting

  • Lighting (Exterior and Park)

  • Lighting (Interior)

  • Loads associated with renewable power source

  • Machine

  • Main/Incomer

  • Mixed usages

  • Office equipment

  • Other

  • Plug loads

  • Process

  • Refrigeration

  • Renewable power source

  • Sockets

  • Special loads

  • Sub/Head of group

  • Total

  • Transportation system

  • Vapor

  • Ventilation

  • Water

  • Water pump system

Zone Management

You can create up to 50 zones and assign devices to each zone to enable you to view data associated with a specific zone in your system more easily.

NOTE: Zone data is not published to Cloud or to SFTP or HTTPS servers. Zone data is not exported in a local csv export or through the Trending webpage (Advanced model)

From the device page in Settings, click the zone settings icon next to Zone in Contextualization data. The zone setting table opens. The table displays the list of all created zones and the number of devices associated with each zone.

Zones are displayed in alphabetical order by default. You can display them in reverse alphabetical order by clicking the arrow in the Zone name header. You can also display them in order of number of associated devices by clicking the arrow in the Associated devices header.

From the table you can perform the following actions:

  • Create a new zone: enter the name of the new zone in the empty cell at the bottom of the table. A zone name can be up to 50 characters in length and can contain letters, numbers, spaces and/or special characters. A message pops up to inform you if the zone name already exists. Click on the ✔ to add the new zone to the table.

  • Modify a zone name: click the edit icon (). Enter the new name and click ✔. The name is automatically updated for all associated devices.

  • Delete a zone: click the bin icon (). A popup message requires you to confirm that you wish to delete the zone. Devices previously assigned to this zone are no longer associated with a zone.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.