DOCA0172EN-20

Appendix D: SFTP and HTTPS Publication File Formats

CSV Publication

The following table provides the details of each row of the .csv file, with sample data:

Row

Data in .csv file

Description

1

“Gateway Name”,”Gateway SN”,”Gateway IP Address”,”Gateway MAC Address”,”Device Name”,”Device Local ID”,”Device Type ID”,”Device Type Name”,”Logging Interval”,”Historical Intervals”

This row contains the column headings for the information provided in row 2:

  • Gateway Name: name given to Panel Server during commissioning

  • Gateway SN: serial number of Panel Server

  • Gateway IP: IP address of Panel Server

  • Gateway MAC Address: MAC address of Panel Server

  • Device Name: name given to the device during commissioning

  • Device Local ID: reference of the logged device, unique across Panel Server

  • Device Type ID: device model

  • Device Type Name: device model

  • Logging Interval: sampling period expressed in minutes

  • Historical Intervals: total number of rows of logged data in this file

2

“Device TypeEcoStruxure Panel Server”,”542206310926”,”10.195.253.81”,”00:00:54:E5:8A:36”,”F160 3P 3P+N”,”modbus:1_mb_81”,”F160 3P 3P+N”,”F160 3P 3P+N”,”5”,”7”

This row contains information about the Panel Server that produced the file, and the downstream device from which the measurements were sampled.

3

4

“ “,” “,” “,”Topic ID1”,”Topic ID2”

This row contains the column headings for the topic IDs. A topic ID is a reference to the quantity being logged. The name given to a quantity may differ between devices and languages. Topic IDs are used to identify the quantity regardless of the device or language. Topic IDs are unique across the Panel Server.

NOTE: The first 3 commas are used for layout purposes in a spreadsheet application.

5

“ “,” “,”“,"modbus:1_mb_VAB","modbus:1_mb_VAN"

This row contains the topic IDs of the measurements logged.

6

7

“Error”,”UTC Offset (minutes)”,”Local Time Stamp”,”RmsVoltagePhsAB (V)”,”RmsVoltagePhsAN (V)”

This row contains the column headings for the data logged in rows 8 and more:

  • Error: 0 for success, 19 when at least one measurement was invalid or not available for sampling (NaN).

  • UTC Offset (minutes): offset of local timestamp from UTC timezone.

  • Local Time Stamp: date and time of the samples

From the fourth item onward, each measure is described by its name and unit (if known).

8 and more

“0”,”0”,”2022-11-04 08:10:00”,”127.80000305”,”235.3999939”

“0”,”0”,”2022-11-04 08:15:00”,”128.1000061”,”235.69999695”

“0”,”0”,”2022-11-04 08:20:00”,”127.69999695”,”234.8999939”

These rows contain the logged data.

JSON Publication

The following table provides an explanation of the .json file content, with example content taken from the example file to illustrate.

Data in json file Description Example

valueItemId

Device name and measurement/event. The device name used in the .json file is an internal name. To get the correspondence between this name and the device name listed in the Panel Server, follow the procedure to export all logs. The diagnostic_topology.txt file in the exported logs lists device names and internal names.

Io_block:7_iod_827_DO1 denotes IO device number 7, and the record of the actions on Digital Input 1

timestamp

Time reference of beginning of sampling period

2023-03-28T08:13:00Z

v

Measurement/event

Open

t

Time offset in ms to add to time reference

120000 ms = 120 s = 2 min so sample taken at 08.13 + 2 min = 08.15

s

Invalid measurement

false

The following lines provide an example of a .json file with data consisting of a list of two time series with a collection of several records:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.