DOCA0172EN-20

Alarm File

The alarms available on the Panel Server webpages depend on the device type. For details about alarms available on each device, refer to spreadsheet DOCA0330EN EcoStruxure Panel Server - Alarm File or refer to the user guide of the selected device.

IMPORTANT:
  • Concerning IO module generic function, alarm activation is enabled when the input status is 1.

  • When Acti9 iATL24, OFSD or iACT24 auxiliaries are connected under an I/O Smart Link device and commissioned in the Panel Server, if the cable is disconnected from the I/O Smart Link device, a Circuit breaker opened alarm is triggered into the Panel Server instead of the Communication loss alarm.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.