DOCA0172EN-20

Configuration of Exiway Link Devices

Presentation

Exiway Link devices are wireless emergency lighting devices.

Configuration Procedure

To configure Exiway Link devices follow the procedure in Configuring Wireless Devices Through Webpages:

Parameter Tables

Identification

Refer to Configuring Wireless Devices Through Webpages.

Modbus virtual

Refer to Configuring Wireless Devices Through Webpages.

Contextualization data

Refer to Configuring Wireless Devices Through Webpages.

Removing Exiway Link Devices

NOTICE
Hazard of incorrect REMOVAL of devices on a shared network
  • Before removing an Exiway Link device, check if other devices on the same network may be impacted.
  • Remove devices in the correct order if they are part of a mesh architecture.
Failure to follow these instructions may result in incorrect functioning of devices.

Exiway Link devices can be part of a mesh network. Removing one device on this network can have an impact on other devices. If you need to remove all devices, ensure that you remove them in the correct order.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.