DOCA0172EN-20

Configuration of Ambient Sensors Through Webpages

Presentation

Ambient sensors can be configured through Panel Server webpages.

For a complete list of supported ambient sensors, refer to the respective release notes:

  • DOCA0249•• EcoStruxure Panel Server Entry - Firmware Release Notes

  • DOCA0178•• EcoStruxure Panel Server Universal - Firmware Release Notes

  • DOCA0248•• EcoStruxure Panel Server Advanced - Firmware Release Notes

Configuration Procedure

To configure ambient sensors, follow the procedure in Configuring Wireless Devices Through Webpages.

Depending on the sensor, if necessary, during the configuration procedure, identify the specific sensor in its location by clicking Start in Locate. The sensor LED blinks for 30 seconds. This enables you to select the required sensor to modify its configuration.

Parameter Tables

Identification

Refer to Configuring Wireless Devices Through Webpages.

Communication Settings

Parameter name Description

Communication period (s)

When available for the selected wireless device, you can set the communication period at a value different from the value set at family devices level. Select a value of between 60 and 600 seconds from the list. The change is applied at the next communication with the device.

Modbus virtual

Refer to Configuring Wireless Devices Through Webpages.

Contextualization data

Refer to Configuring Wireless Devices Through Webpages.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.