DOCA0172EN-20

Settings Menu

Settings Menu Structure

  • * Not available on Wired by Design models.
  • Available on all models.
  • Available on Universal and Advanced models.
  • Available on Advanced models.

For more information, refer to Settings menu.

Settings Menu Description

NOTICE
IMPAIRED NETWORK PERFORMANCE
Only qualified personnel should modify the Ethernet and/or Modbus-SL settings. Perform such modifications only after you have read about and understood the Ethernet and/or Modbus-SL settings.
Failure to follow these instruction can result in loss of network connectivity

The webpage for the Settings menu displays the cards and sub-menus for configuration and communication settings. The cards and sub-menus on the webpages depend on the Panel Server model.

Card

Sub-menu

Description

General

Identification

Information about the Panel Server identification:

  • Device name

  • Device range

  • Device model

  • Commercial reference

  • Serial number

  • Hardware revision

  • Firmware revision

Date & Time

Used to set the date and time manually or via NTP (Network Time Protocol).

Network communication

Ethernet

Allows you to configure the Panel Server Ethernet mode including ports and IP parameters (IPv4 and IPv6).

DNS

Allows you to configure the DNS server.

RSTP

Allows IT specialists to configure RSTP protocol.

DPWS

Allows you to configure the IP network discovery.

Proxy

Allows you to configure the Internet proxy settings.

Wi-Fi infrastructure

Allows you to configure the Wi-Fi settings.

Wi-Fi access point

Allows you to configure the Wi-Fi access point settings.

Services

Communication services activation: Allows you to enable or disable the following services per interface :

Modbus TCP/IP:

  • in switched mode

  • on ETH1 port in separated mode

  • on ETH2 port in separated mode

  • on Wi-Fi

Modbus devices

Modbus configuration

Allows you to define the Modbus-SL and Modbus TCP/IP network.

Custom models

Allows you to upload Modbus-SL and Modbus TCP/IP devices that are not natively managed by the Panel Server built-in models.

Displays a link to access EPC Web tool directly to create custom device models.

Device addition

Allows you to discover the Modbus-SL and Modbus TCP/IP devices by using a selective list.

Registers read

Allows you to troubleshoot the addition of Modbus devices.

Modbus devices

Detailed information about each device in the Modbus network. Information (for example, device identification, custom model name and version, electrical characteristics) and contextualization data (entered by the user) depend on the device type.

Wireless devices

Network configuration

Allows you to define the IEEE 802.15.4 network when activated.

Discovery

Allows you to discover the wireless devices in the IEEE 802.15.4 network by using a selective list or non-selective discovery.

Global functional settings

Allows you to :

Wireless devices

Allows you to send a Locate command to make the wireless device blink for 30 seconds (5 minutes for Exiway Link devices).

Provides detailed information about each wireless device in the IEEE 802.15.4 network. Information (for example, device identification, device RF-ID, electrical characteristics, Modbus virtual server ID) and contextualization data (entered by the user) depend on the device type.

Embedded Input Management

I/O configuration

Allows you to configure the Panel Server digital inputs.

Embedded input

Allows you to configure inputs/outputs of I/O devices associated with Panel Server.

Data Management

Data sampling

Allows you to define data sampling of the connected devices.

Local export

Allows you to export the data sampled locally in a .csv file. (Available in Advanced model only.)

Device tree view

Detailed information about sampling for each device connected to the Panel Server. Devices are sorted by usage or zone. Select the means to group the devices in the list by clicking the list icon .

Measurements and alarms depend on the device type.

Data Publication

Data Publication

Allows you to set the means used to publish data and to enable the email of alarms service.

Security

Network management

Allows you to configure the security feature to permanently disable the wireless networks.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.