DOCA0172EN-20

Removing Modbus Devices Through Webpages

Presentation

It is possible to remove Modbus devices from the Panel Server system. This allows you to discover the device from another Panel Server, for example.

Removal Procedure

Follow this procedure to remove Modbus devices from the system:

  1. Navigate to Settings > Modbus devices > Modbus devices to view the list of connected devices.

  2. Select the device to be removed from the system.

  3. Click the bin icon on the top right side of the webpage.

  4. Confirm removal process.

    Result: Once the Modbus device is successfully disconnected from the Panel Server, it is no longer visible in the list of Modbus devices.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.