DOCA0172EN-20

Home Menu (Advanced Model)

The webpage for the Home menu displays the consumption of energy of the system managed by the Panel Server.

By default, the consumption of electricity is displayed for a period of one day (yesterday, day before yesterday) in two pie-charts. Other commodities and periods can be selected. Consumption charts are organized:

  • By usage

  • By zone

In each case, the top five consumers are displayed, arranged from highest to lowest consumption. Other consumers of the selected commodity are displayed as a sixth category, labelled Miscellaneous other usages or Miscellaneous other zones, depending on the chart. Main consumers are calculated based on consumption over Period 1.

A pie-chart shows the distribution of the top five consumers, with all other consumers grouped into a sixth category. The webpage displays for each consumer:

  • The consumption of period 1

  • The change in consumption over period 1, compared to period 2 (as a percentage)

  • The trend: increasing, decreasing (indicated by an arrow icon),or flat (no icon)

You can click on the name of a consumer in the legend to the right of the chart to get detailed information about that consumer.

In the Home page you can select a different commodity (for example, gas) and a different period (one day, one week, or 4 weeks). For more information about settings, see Consumption Overview.

When you are logged into the Panel Server webpages, the Home page automatically displays if historized data is available.

For more information about trending data, click the Trending icon:

  • In By Usage to go to Trending > Aggregated view by usage

  • In By Zone to go to Trending > Aggregated view by zone

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.