DOCA0172EN-20

Network Settings

Overview

Panel Server features wired and wireless communication and enables network communication. The Panel Server offers the following connection interfaces:

  • Ethernet:

    • One port on Entry model

    • Two ports on Universal and Advanced models

  • Wi-Fi (except Wired by Design models)

Availability

This function is available on Panel Server Entry, Universal, and Advanced.

Setting the Parameters

The network configuration is set as follows:

  • With EcoStruxure Power Commission software

  • On the Panel Server webpages, at Settings > Network communication.

Select the appropriate network configuration for your system. If necessary, enter the parameters for each connection interface displayed.

For detailed information about a network configuration option and settings, see:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.