DOCA0172EN-20

EcoStruxure Panel Server Webpages Overview

The web server embedded in the EcoStruxure Panel Server provides webpages enabling you to commission electrical products and systems compatible with the EcoStruxure Panel Server in your switchboard.

In addition the webpages provide real-time data and active alarm visualization, and historical analysis from devices (depending on the model), for entry-level energy and operation management.

Electrical product and commissioning capabilities allow you to:

  • Discover wireless devices installed in the EcoStruxure Panel Server system (depending on the model).

  • Discover Modbus-SL and Modbus TCP/IP devices from EcoStruxure Panel Server (depending on the model).

  • Configure I/O devices connected to the EcoStruxure Panel Server through the digital inputs (depending on the model).

Energy and operation monitoring capabilities allow you to:

  • Visualize real-time data and events through a supported web browser.

  • Monitor and control connected devices.

  • Publish data to an SFTP or HTTPS server or to the Schneider Electric cloud.

  • Visualize trending on historical data, up to a period of 3 years (Advanced model).

  • Export selected logged data to your PC for additional analysis (Advanced model).

For more detailed information about the webpages, refer to Using EcoStruxure Panel Server Webpages.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.