DOCA0172EN-20

Publication on SFTP Server and Email Notification for Alarms (Advanced Model)

Presentation

This service combines the publication to SFTP server and email notification for alarms.

For more information on each individual service, see the detailed topic:

Availability

This function is available on Panel Server Advanced.

Setting the Parameters

Publishing function is set on the EcoStruxure Panel Server webpages, at Settings > Data publication > Publication method > SFTP & Email for alarms.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.