General Principle to Commission an EcoStruxure Panel Server
Overview
The commissioning of an Panel Server can be performed using one of the following tools:
-
EcoStruxure Power Commission software. See EcoStruxure Power Commission Online Help.
Use the software for a system-focused, global approach to configure the Panel Server and all the devices in the switchboard. In addition, the software advanced features allow you to:
-
prepare a project off-line.
-
save a project (system configuration).
-
create a new project from an existing one.
-
generate a report with data collected during configuration testing and to retrieve the settings updated through the Panel Server webpages.
-
to export a project to a supervision software (for example, EcoStruxure Power Monitoring Expert).
-
-
Use the webpages for a device-focused approach to
-
add or remove Modbus and/or wireless devices
-
configure or modify settings of connected devices
-
set up data contextualization of connected devices
-
set up data sampling and data publishing
-
export data to files
-
-
EcoStruxure Power Commission Mobile app in conjunction with EcoStruxure Energy Hub (part of EcoStruxure Building Activate).
Use the app for a device-focused commissioning of a limited selection of settings through a Wi-Fi connection. For more information, refer to the detailed topic.
During commissioning of the Panel Server through an Ethernet connection, update the firmware of the Panel Server.
Pre-requisites to Commissioning
To commission the Panel Server with EcoStruxure Power Commission software or Panel Server webpages, use one of the following connection methods:
-
Connect the Panel Server to Ethernet (see Connection to a PC).
-
Connect a PC to the Panel Server through the Wi-Fi access point (see Connecting to the Wi-Fi Access Point from a PC).
To commission with EcoStruxure Power Commission Mobile app, connect to the Panel Server Wi-Fi access point.