DOCA0172EN-20

EcoStruxure Power Commission (EPC) Software

Overview

EcoStruxure Power Commission is intelligent software that helps you set up, test, and commission the electrical products and systems in your switchboards with efficiency and ease. It also allows you to generate a dedicated QR code for the electrical panel to enable digital collaboration with contractors and facility managers by sharing important documentation.

Key Features

EcoStruxure Power Commission software performs the following actions for the supported devices :

  • Easy setup

    • Discover all the smart devices in your electrical switchboard

    • Check firmware compatibility and install upgrades as required

    • View communication architecture and adjust communication settings

    • View the list of devices organized in the switchboard, and configure electrical settings for breakers and meters

  • Advanced testing

    • Execute Factory Acceptance Tests (FAT) and reporting:

      • Test MasterPacT MTZ circuit breakers with automatic trip curve tests, zone-selective interlocking tests

      • Test the communication wiring and generate reports

  • Fast commissioning

    • Adjust settings without connection to the devices through offline configuration feature

    • Use batch operations features to speed up settings configuration, for several devices at the same time

    • Generate a comprehensive project report that lists your switchboard and related devices, firmware version, and serial numbers, for example.

  • Digital collaboration

    • Create a unique QR code for the entire switchboard and then upload all relevant documentation including important CAD drawings, user guides, bill of materials, single-line diagrams, photos and more to Schneider Electric cloud repository.

    • Simplify project handover with the digital logbook functionality, making it faster and easier for the facility manager to access historical information and collaborate with all project partners

For more information, tutorials, and download link, visit the EcoStruxure Power Commission software webpage.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.