Backup and Restore Panel Server Configuration
Presentation
At any moment after commissioning, the configuration of a Panel Server can be saved into a file and used to restore the configuration in a Panel Server of the same model and hardware version, or the same Panel Server.
Note that the backup and restore function enables you to restore a Panel Server configuration only. There is no backup or restoration of sampled data. When the restore function is executed, all logged data is flushed. Export any data before executing the restore function to avoid losing it.
Schneider Electric recommends that you encrypt the backup file with a password to help secure sensitive information. Safeguard the backup file in a protected location to prevent unauthorized access.
| NOTICE |
|---|
|
Unauthorized data access
Failure to follow these instructions can result in equipment damage.
|
Data related to commissioning is stored in the backup file, for example:
-
Commissioning data
-
System settings including date and time, networks (Ethernet, Wi-Fi), DPWS, Modbus-SL, Proxy, and Schneider Electric cloud platform activation status
-
IEEE 802.15.4 network settings and status
-
End-device settings and contextualization, including Modbus-SL, Modbus TCP/IP, IEEE 802.15.4, and inputs/outputs
-
Data sampling settings and contextualization
-
Events and alarms settings including notification configuration per alarm.
-
-
Custom models
The backup file only contains data that allows you to restore an installation back to a previous state, that is, the state it was in when generating the backup file. Therefore, it does not include data unrelated to commissioning, for example:
-
Setting of Remote control and scheduling from cloud function
-
Logs including diagnostics counters and diagnostics logs
-
Firmware revision of the Panel Server
-
SFTP server password and SFTP server key fingerprint. These settings need to be entered again after a restore operation.
Availability
This function is available on Panel Server Entry, Universal, and Advanced.
Setting the Parameters
-
With EcoStruxure Power Commission software
-
On the EcoStruxure Panel Server webpages, at
Panel Server Configuration Backup Settings
The following table describes the settings available from the webpages.
|
Parameter |
Description |
|---|---|
|
Backup |
Used to save the Panel Server configuration. |
|
Backup settings |
Used to name the backup file and help secure backup data by encrypting the backup file with a password. IMPORTANT: The file password
is stored irreversibly. If you do not remember the password, the configuration
backed up in the file becomes unusable.
|
Panel Server Configuration Restore Settings
The following table describes the setting where it is available.
|
Parameter |
Description |
|---|---|
|
Restore |
Used to restore configuration from a backup file. Check that the Panel Server receiving the backup meets the following conditions:
IMPORTANT: A backup file from a different Panel Server can be restored only once and on only one Panel Server.
When the configuration is restored in the Panel Server, an error message may be displayed. The message indicates that the number of Modbus devices on the current Panel Server differs from the number of Modbus devices on the previous Panel Server when configuration was backed up. IMPORTANT: When
the configuration is restored, remote control (and scheduling from
cloud) is deactivated by default and existing logged data is flushed.
|
Restoring Configuration With Wireless Networks Permanently Disabled
The permanent deactivation of the wireless networks is not saved in the Panel Server backup file.
Setting this feature depends on the type of restored Panel Server:
|
If... |
Then... |
|
Data is restored in a new Panel Server |
The wireless networks are enabled by default. If permanent deactivation is required as in the backed-up Panel Server, follow the procedure. |
|
Data is restored in the same Panel Server |
Wireless networks remain deactivated. |