DOCA0172EN-20

Diagnostics

Presentation

Diagnostics data provides statistical data about the Panel Server and connected devices. The events are gathered by type of application: cloud connection, Modbus Serial network, and wireless network.

Availability

This function is available on Panel Server Entry, Universal, and Advanced.

Setting the Parameters

Diagnostics are set on the Panel Server webpages:

EcoStruxure Panel Server Diagnostics

Parameter Description
Ethernet information

Ethernet information switched port

  • ETH1 link status

  • ETH1 Duplex transmission speed information

  • ETH1 Duplex transmission information

  • ETH2 link status

  • ETH2 Duplex transmission speed information

  • ETH2 Duplex transmission information

  • Received frames

  • Transmitted frames

  • Received errors

  • Transmitted errors

  • Transmitted collisions

Modbus serial client counter information

Displays diagnostics counters for Modbus-SL protocol:

  • Received messages

  • Transmitted messages

  • Messages timeout

  • Protocol errors

  • Received exceptions

  • Cyclic Redundancy Check (CRC) errors

Reset counters button allows you to reset the counters to zero.

Modbus TCP/IP server connection information

Displays connection information for Modbus TCP/IP protocol:

  • Number of active connections

  • Maximum number of connections allowed

  • Maximum number of simultaneous connections occurred

  • Failed connection counter

Reset counters button allows you to reset the counter to zero.

Modbus TCP server counter information

Displays message counters for Modbus TCP/IP protocol:

  • Received messages

  • Transmitted messages

  • Protocol errors

Reset counters button allows you to reset the counters to zero.

Wireless (802.15.4) identification*

Displays identification of IEEE 802.15.4 wireless network:

  • RF-ID

  • Personal Area Network (PAN) identifier

  • Extended PAN identifier

  • Network address

Wireless (802.15.4) network status*

Displays status of the IEEE 802.15.4 wireless network

  • Network status

Modbus Devices Diagnostics

Parameter Description
Modbus information

Displays identification and diagnostics counters for Modbus devices:

  • Server identifier historical data (1–254)*

  • Received messages

  • Transmitted messages

  • Protocol errors counter

  • Message timeout counter

  • Received exceptions counter

  • Connection timeout counter

  • Detail of received exceptions

Reset device counters button allows you to reset the device counters to zero.

The table of channels displays information about Input 1 and Input 2 devices, where relevant.

Wireless Devices Diagnostics

Parameter Description
Modbus identification*

Displays Modbus identification:

  • Virtual server identifier (1–254)

Wireless network indicator*

For more information, see Appendix C.

Displays connection information of the wireless devices:

  • Signal quality level

    • Weak

    • Fair

    • Good

    • Excellent

    For information about how the signal quality level is calculated, see Appendix C.

  • Device indicator

    • Device received signal strength indicator (RSSI)*

    • Device link quality indicator (LQI)*

    • Device packet error rate (PER)*

  • Panel Server indicator

    • Device received signal strength indicator (RSSI)

    • Device link quality indicator (LQI)

    • Device packet error rate (PER)*

  • Link indicator

    • Device received signal strength indicator (RSSI)

    • Device link quality indicator (LQI)

    • Device packet error rate (PER)*

Status Power source

Displays power source of the wireless devices.

Power source backup*

Displays backup power source of the wireless devices, where relevant.

Inputs/output*

Displays the following information:

  • Name

  • Label

  • Status Input

Embedded Input Device Diagnostics (PAS600L, PAS600LWD and PAS800L Models)

Parameter Description

Embedded input

For digital input configured as Pulse counter, displays Raw counter value.

For digital input configured as Standard input, displays Status.

System Monitoring Diagnostics

Parameter Description
Health state

Uptime indicates how long the Panel Server has been running for.

Health state indicates the Panel Server state:

  • Nominal

  • Degraded: If the Health state is indicated as Degraded, a table indicates the possible causes of the degradation, refer to table below.

Global performance

Displays Panel Server performances:

  • CPU usage (in %)

  • Memory usage (in %)

The following table shows examples of possible causes of health state degradation:

Topic Level Date

Lost communication with Modbus serial device(s)

Indicates the level of severity of the cause.

Indicates the date and time the degraded state occurred.

Lost communication with Modbus TCP/IP device(s)

Lost communication with wireless device(s)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.