DOCA0172EN-20

IEEE 802.15.4 Communication

Presentation

In an EcoStruxure system where IEEE 802.15.4 wireless devices are connected to a Panel Server, these wireless devices are required to withstand EMC levels as per IEEE 802.15.4 standard for proper device performance. For details about supported Schneider Electric IEEE 802.15.4 wireless devices, refer to the relevant Panel Server firmware release notes:

  • DOCA0249•• EcoStruxure Panel Server Entry - Firmware Release Notes

  • DOCA0178•• EcoStruxure Panel Server Universal - Firmware Release Notes

  • DOCA0248•• EcoStruxure Panel Server Advanced - Firmware Release Notes

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Use IEEE 802.15.4 communication only with ComPacT, PowerPacT, MasterPacT MTZ, and other qualified devices.
Failure to follow these instructions will result in death or serious injury.

IEEE 802.15.4 wireless communication devices provide a compact and high-density metering solution with numerous and accurate data for building systems. These wireless devices can send temperature, humidity, energy, power, current, voltage, and power factor to the Panel Server.

Wireless devices are connected downstream to the Panel Server.

All wireless devices are connected on the same channel. If you change the channel, the wireless devices scan other nearby channels until they reestablish communication with the Panel Server. The scan function can be disabled on compatible devices if required. Refer to Managing the Channel Scan.

The maximum number of wireless devices that can be connected to one Panel Server is detailed in the related topic.

The Panel Server Universal (hardware version 002.000.000) and Panel Server Advanced can be connected to an external IEEE 802.15.4 antenna to extend the wireless network.

Availability

This function is available on Panel Server Entry, Universal (except Wired by Design models), and Advanced.

Setting the Parameters

IEEE 802.15.4 communication function is set as follows:
  • With EcoStruxure Power Commission software

  • On the Panel Server webpages, at Settings > Wireless devices > Network configuration

Configuration Settings

WARNING
UNINTENDED EQUIPMENT OPERATION OR ALTERED FEATURE OF PROTECTIVE DEVICES
When installing a Panel Server in a metallic enclosure, and connecting it to an external IEEE 802.15.4 antenna, do not install this antenna within the enclosure.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Correct operation of protective devices installed in a metallic enclosure can be altered by a high level of IEEE 802.15.4 network radio frequency transmission power.

The following table describes the settings available from the webpages.

Parameter Settings Description
Wireless network settings Wireless activation

Used to enable/disable wireless emission of the Panel Server (disabled by default).

Channel mode

Used to specify how the IEEE 802.15.4 channel is selected:

  • When you select Auto (default setting), the most appropriate channel is automatically selected by the Panel Server.

  • When you select Manual, configure the wireless parameters:

    1. Enter the required channel (value between 11 and 26)

    2. Save your settings by clicking the icon at bottom right of the screen and selecting Save.

NOTE: When ZBRT devices are connected to the Panel Server, decommission and remove the ZBRT devices before changing the channel mode or channel number, and add them again after the change.

Channel

Enter the channel number.

Antenna selection

Used to select the type of IEEE 802.15.4 antenna used in the architecture:

  • Internal (Panel Server internal antenna) (default setting)

  • External (Panel Server external antenna, Panel Server Universal hardware version 002.000.000 and Advanced model option)

  • Both (internal and external antennas are used with Panel Server Universal hardware version 002.000.000 and Advanced.)

Output power

Output power level cannot be changed when the internal antenna or both antennas (internal and external) are used.

Output power can be set only when an external IEEE 802.15.4 antenna is connected to a Panel Server Advanced:

  • If Antenna selection is set to Internal or Both, the internal antenna is used and Low level is displayed (setting not editable).

  • If Antenna selection is set to External, set the output power to Low level or High level depending on your network.

NOTE: When a Panel Server connected to an external IEEE 802.15.4 antenna is installed in a metallic enclosure, check that the antenna is not installed within the enclosure.

Dynamic antenna selection

(Available when Internal is selected in Antenna selection.)

Dynamic antenna selection

An advanced feature to be used with caution. Disabled by default. Refer to Manage dynamic antenna selection.

Used to enable the Panel Server to switch between internal antennas, based an analysis of the signal quality.

The following fields are displayed when Dynamic antenna selection is enabled.

Automatic analysis

Enabled by default. Used to enable automatic launch of analysis when the Panel Server detects a communication loss with a TH110 or CL110 sensor.

Launch analysis/Stop analysis

Used to start an analysis or stop an analysis that is in progress.

NOTE: Check that TH110 and CL110 sensors are powered on before launching an analysis.

Analysis status

Indicates the status of the analysis:

  • In progress

  • Successful

  • Canceled

Analysis result

Indicates which antenna is selected after the analysis is done:

  • AntennaA

  • AntennaB

  • Antenna switching mode

Wireless communication

For more information about setting the communication period, refer to Setting the Communication Period for Device Family.

Communication period for ambient sensors (s)

Used to set the communication period for the ambient sensor family. Select a value between 60 and 600 seconds from the list.

Default setting: 120 seconds

NOTE: The ambient sensor family includes any type of environmental sensor, for example, HeatTag, TH110, CL110.

Communication period for control devices (s)

Used to set the communication period for the control device family. Select a value between 5 and 120 seconds from the list.

Default setting: 60 seconds

Communication period for energy related devices (s)

Used to set the communication period for the energy related device family. Select a value between 5 and 120 seconds from the list.

Default setting: 15 seconds

Network occupancy

Indicates the network occupancy as a percentage.

Wireless device management

Remove all devices

Used to remove all wireless devices connected to the Panel Server.

Manage scan function

Scan activation

Used to enable or disable scan function of wireless devices (enabled by default). Refer to Managing the Channel Scan Function.

  • Status on wireless device: indicates the result of the change to the scan function.

  • Retry: button used to try to enable or disable the function again after an unsuccessful attempt, with status displayed as Not applied on all devices.

Setting the Communication Period for Device Family

The communication period defines the frequency (in seconds) at which each wireless device sends data to the Panel Server. This is only applicable to real-time data and not to alarms that are immediately notified in case of event.

Set the communication period for all discovered devices that support this feature, and for each family of devices.

Any change to the communication period takes time to be applied on devices, as it is not applied until the next communication with the device.

NOTE: If the communication period is reduced, it can potentially impact the stability of the wireless network, and indicator of radio quality may be degraded. Use the network occupancy information to help you understand the impact of the changes. As standard, the Panel Server has a defined default value for each family of wireless devices.

The communication period can be changed as follows, if needed:

  1. Select the required communication period from the Communication Period list.

  2. Save your settings by clicking the icon at bottom right of the screen and selecting Save. The communication period updates in the webpages. A command to change the communication period is sent to each connected device. For each device the change is applied at its next communication with the Panel Server.

    NOTE: On the settings page for each individual device to which the change is relevant, the change may take up to three times the original communication period to be updated. During this time you may observe one of the three following results in the Communication period (s) field:
    • The communication period is updated to the new setting. The Panel Server communicated with the device.

    • A spinner icon with the text Updating device is displayed. The Panel Server is in communication with the device.

    • The communication period is not updated to the new setting. The Panel Server has not yet communicated with the device.

Settings of Wireless Devices Discovery

The following table describes the settings available in the Panel Server webpages.

Parameter Settings Description
Discovery

Discovery method

  • Automatic (enabled by default): Used to discover any available devices.
  • Selective: Used to discover a selective list of wireless devices to be connected to the Panel Server.
  • Click Upload file to import a prepared selective list in CSV format.
  • Protect Plus (enabled by default): Enable this function for a selective discovery process with heightened security for 16-character RF-ID devices, using the install code
  • Click Start to launch the discovery.

For more information, refer to Discovery of Wireless Devices Through Webpages

Discovery result Discovery status

Indicates the status of the device discovery on the wireless network:

  • Idle: device discovery is inactive.

  • InProgress: device discovery is in progress

  • Done: device discovery is performed.

Discovery

Table displaying the discovered wireless devices with device picture, name, and RF-ID.

Rejected discovery

Table displaying the wireless devices for which the discovery was not successful. A Status column indicates the cause of the rejected discovery.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.