DOCA0172EN-20

Device Configuration with EcoStruxure Power Commission Mobile App

It is possible to configure a wireless device by using EcoStruxure Power Commission Mobile app, in conjunction with EcoStruxure Energy Hub (part of EcoStruxure Building Activate), connected via the Wi-Fi access point. For more information, follow the on-screen instructions in the app.

The following configuration settings are available:

  • General

  • Network communication

  • Wireless devices

  • Data publication

For more information about EcoStruxure Power Commission Mobile app, refer to DOCA0366EN EcoStruxure Power Commission Mobile Application - User Guide.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.