DOCA0172EN-20

Configuring Smart Link Modbus Channels

Presentation

For Smart Link devices configured in the Panel Server webpages, you can configure each of the available channels at Settings > Modbus Devices > Configuring channel settings. The following information is displayed:

Parameter name Description

Data status

Indicates the status of the data.

Last synchronization status

Indicates if the last synchronization was successful.

Refresh the configuration

Click on this button to refresh the configuration.

Table indicating channel configuration

Columns in the table display the following information for each channel:

  • Channel number

  • Input 1 name

  • Input 2 name

  • Output name

Procedure to Configure Channels

Follow this procedure to configure channels:

  1. Click on the pencil icon to open the configuration for a channel.

    Result: Editable fields open below the channels table.

  2. Select the I/O Type from the following list:

    • Not connected

    • Wired device

    • Pulse counter

    • Standard I/O

    The settings shown below are for configuration of a Wired device. The settings for Pulse counter and Standard I/O are the same as those for the Panel Server digital inputs, which are described in the specific topic.

  3. Select the Device Type for Input 1.

    NOTE: If you select OF24 as the Device Type, you need to enter data for Input 2 in addition.

  4. Enter the data for Input 1 in the fields, referring to the following table for more information about the parameters.

Parameter Tables

Input 1

Parameter Description

Name

Enter the input name of the device.

Label

Enter the input label.

Commodity

Select the commodity type in the list, as contextualization data.

Usage

Select the usage in the list, as contextualization data.

Zone

Select the zone in the list, as contextualization data.

Click the Settings icon to:

  • Create a new zone

  • Modify a zone name

  • Delete a zone

For more information about creating, modifying and deleting zones, refer to Zone Management.

I/O Contextualization with I/O type Standard I/O

Select the contextualization data in the list.

NOTE: Refer to the following table for interpretation of Meaning of input = 0 and Meaning of input = 1 for certain signal elements.

For inputs configured as Standard I/O, the following I/O Contextualization selections, display a result for Meaning of input = 0 and Meaning of input = 1 that should be interpreted as shown in the table below. For other I/O Contextualization selections, the result displayed requires no interpretation.

Contextualization (Signal element) Displayed Interpretation
Meaning of input = 0 Meaning of input = 1 Meaning of input = 0 Meaning of input = 1

Trip indicator status (SD)

On

Off

In fault

No fault

Electrical trip indicator status (SDE)

On

Off

In fault

No fault

Earth leakage fault

On

Off

In fault

No fault

Ground fault

On

Off

In fault

No fault

Forced freewheel stop

Off

On

Inactive

Active

Battery status

OK

Error

OK

In fault

Advanced protection

In fault

No fault

In fault

OK

Motor preheating

Off

On

Off

Preheat

UPS status

OK

Error

OK

In fault

UPS running mode

Supplying

Standby

Supplying

By pass

Under temperature

NotUnderTemperature

UnderTemperature

Inactive

Active

Over temperature

NotOverTemperature

OverTemperature

Inactive

Active

Equipment status

Stopped

Running

Stop

Start

Tariff status (1–5)

Off

On

Inactive

Active

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.