DNS
Presentation
TCP/IP communication is used to perform commissioning, data collection and data publishing, and connection to supervision software.
TCP/IP communication general principles, such as DNS and proxy settings, apply to Ethernet and Wi-Fi.
Domain Name System (DNS) is the naming system for PCs and devices connected to a local area network (LAN) or the Internet.
The following features require DNS service:
-
Cloud connection.
-
HTTP/HTTPS proxy if a domain name is used.
-
SFTP if a domain name is used.
-
NTP if a domain name is used.
Availability
This function is available on Panel Server Entry, Universal, and Advanced.
Setting the Parameters
-
With EcoStruxure Power Commission software
-
On the Panel Server webpages, at
DNS Settings
The following table describes the settings available from the webpages.
| Parameter | Description |
|---|---|
| DNS assignment mode | Used to select
the DNS server configuration mode:
|
| Primary DNS server | Used to enter manually the IPv4 address of the primary DNS server when the parameter DNS configuration mode is set to Static. |
| Secondary DNS server | Used to enter manually the IPv4 address of the secondary DNS server when the parameter DNS configuration mode is set to Static. |