DOCA0172EN-20

Publication on HTTPS Server

Presentation

EcoStruxure Panel Server provides a secure connection to an HTTPS server with a certificate authority.

When data sampling and publication to HTTPS are activated, the sampled data of devices is published to the HTTPS server in json or csv files. A maximum of one month of data (Entry or Universal) or three months of data (Advanced) is published to the HTTPS server. If data sampling was activated before this period, older data is not published.

When HTTPS publication is active, data publication on cloud services or SFTP is not available.

Availability

This function is available on Panel Server Entry, Universal, and Advanced.

Setting the Parameters

Publishing function is set on the Panel Server webpages:

  • For Panel Server Entry and Universal at Settings > Data Publication > Publication method > HTTPS.

  • For Panel Server Advanced at Settings > Data Publication > Publication method > HTTPS & Email for alarms

Fill in the Connection information and Publication settings described in the following tables.

HTTPS Publication Settings (Panel Server Entry and Universal)

The following table describes the settings.

Parameter

Settings

Description

Connection information

Server

The host name of the HTTPS server can be defined as the IP address value or as, for example, myHTTPSserver.mydomain.com.

Port

Used to define the HTTPS server TCP port.

Path

Used to enter the path to use on the HTTPS server for data publishing. For example, if /home/user/ is the default directory for the HTTPS server, then the path configured with /myHTTPSPath will publish on /home/user/myHTTPSPath.

Field name

Used to specify the value of the name parameter part of the form-data section included in the file that is being published. By default the filed name is datafile1. The field name is necessary to communicate with the HTTPS server.

Connection method

Radio button used to enable ID authentication.

Username

Used to enter the HTTPS user account name for the user account on the target HTTPS server.

Password

Used to type the password for HTTPS server access.

Test connection

Button used to test the connection to the HTTPS server.

Publication settings

Publication format

Used to select the exported file format:

Publication period

Used to select the publication frequency to the HTTPS server (default setting: 10 min).

NOTE: The publication period is calculated from the end of one publication to the start of the next. The time needed for a publication varies depending on the quantity of data to be analyzed and published.

Start

Button used to launch data publication to the HTTPS server.

HTTPS Publication Settings (Panel Server Advanced)

The following table describes the settings.

Parameter

Settings

Description

Connection information

Server

The host name of the HTTPS server can be defined as the IP address value or as, for example, myHTTPSserver.mydomain.com.

Port

Used to define the HTTPS server TCP port.

Path

Used to enter the path to use on the HTTPS server for data publishing. For example, if /home/user/ is the default directory for the HTTPS server, then the path configured with /myHTTPSPath will publish on /home/user/myHTTPSPath.

Field name

Used to specify the value of the name parameter part of the form-data section included in the file that is being published. By default the filed name is datafile1. The field name is necessary to communicate with the HTTPS server.

Connection method

Radio button used to enable ID authentication.

Username

Used to enter the HTTPS user account name for the user account on the target HTTPS server.

Password

Used to type the password for HTTPS server access.

Test connection

Button used to test the connection to the HTTPS server.

Publication settings

Publication format

Used to select the exported file format:

Publication period

Used to select the publication frequency to the HTTPS server (default setting: 10 min).

NOTE: The publication period is calculated from the end of one publication to the start of the next. The time needed for a publication varies depending on the quantity of data to be analyzed and published.

Include previously historized data toggle switch

Used to include all data for past three months, or from the beginning of data sampling if less than three months.

Start

Button used to launch data publication to the HTTPS server. Refer to Date and Content of the First Data Publication.

Date and Content of the First Data Publication (Panel Server Advanced)

The date and time of the first publication depends on the publication period set, as indicated in the following table.

Publication period First publication date and time and start of data collection

Weekly

00:00 on first Thursday following publication launch

Daily

00:00 following publication launch

12h

00:00 following publication launch

4h

At the next full hour (for example, launch publication at 10:47, publication starts at 11:00)

3h

At the next full hour (for example, launch publication at 10:47, publication starts at 11:00)

2h

At the next full hour (for example, launch publication at 10:47, publication starts at 11:00)

1h

At the next full hour (for example, launch publication at 10:47, publication starts at 11:00)

10 min

At the next interval of 10 minutes (for example, 10:10, 10:20, 10:30 etc)

When the Include previously historized data toggle switch is green, the first publication will contain all the data from the past three months, or from the beginning of data sampling if less than three months.

Connecting to HTTPS Server

To connect the Panel Server to an HTTPS server:

  1. On the HTTPS server, configure a connection for the publication of data from the Panel Server.

  2. In Settings > Network communication > Proxy , click HTTPS proxy and enter the required information.

  3. In the Settings > Data publication webpage, select the Publication method as follows:

    • For Panel Server Entry and Universal select HTTPS.

    • For Panel Server Advanced select HTTPS & Email for alarms

    By default, HTTPS data publications (CSV or JSON file format) are stored at the top of the hierarchical file tree of the HTTPS server. If you customize the file path for the data storage, make sure that the path is created and validated on the HTTPS server. For more information, refer to the user guide of your HTTPS server.

  4. Before connecting to the HTTPS server, fill in the information in the Connection information section. Save your settings by clicking the icon at bottom right of the screen and selecting Save.

  5. Click Test connection.

    NOTE: If it is the first time the Panel Server connects to this HTTPS server, a message appears and requests that you confirm the authenticity of the HTTPS server. Check that your HTTPS server certificate is issued by one of the trusted certificate authorities (Appendix F). Your IT department should be able to provide this information. If the server certificate does not comply, do not publish over HTTPS.
  6. Once the test is performed, the Panel Server webpage displays information:

    • In case of success, a file has been successfully uploaded on the HTTPS server.

    • In case of dysfunction, check the HTTPS server parameters, user credentials, and write access privileges on the HTTPS server.

  7. To publish data, set Publication settings and click Start.

    Result: The sampled data of devices, related to the selected sampling period, is published to HTTPS, in the CSV file format or JSON format. A maximum of one month of data (Entry or Universal) or three months of data (Advanced) is published to the HTTPS server. If data sampling was activated before this period, older data is not published.

  8. If you update the HTTPS server, the HTTPS server fingerprint changes. In this case, click Test connection to allow you to connect to the HTTPS server again.

Disconnecting from Publishing Services

To disconnect Panel Server from the HTTPS server, click Stop.

Disconnecting from the service allows you to connect to another publishing service.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.