DOCA0172EN-20

Sending Commands From Panel Server Webpages

Presentation

You can send commands from EcoStruxure Panel Server webpages.

Output Control Commands to Smart Link Devices

WARNING
UNEXPECTED START OF OPERATION
Only send output control commands for non-critical electrical loads that can safely be left unattended.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Output control commands to I/O Smart Link devices and Acti9 Smartlink Modbus-SL devices can be sent from Panel Server webpages (in data widgets at Monitoring & Control > Input/Output). Open and close commands are used to control non-critical electrical loads.

Individual Commands

Individual commands are executed on one device only. To do this, select a device from the device tree on the relevant webpage, indicated in the list below.

The following functions are available:

  • Locate a wireless device (at Settings > Wireless devices).

    When the Locate button is clicked, the wireless device blinks for 30 seconds. Exiway Link devices blink for five minutes.

  • Reset all energies per device (in data widgets at Monitoring & Control > Wireless devices).

  • Reset peak demand per device (in data widgets at Monitoring & Control > Wireless devices).

  • Send Exiway Link order (in data widgets at Monitoring & Control > Wireless devices).

    • Disable/Enable periodic test.

    • Start functional test.

Global Commands

Global commands are executed on a device family. The command is applied to all the connected devices in the family.

To execute global commands, navigate to Settings > Wireless devices > Global functional settings.

The function allows you to:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.