DOCA0172EN-20

Environmental Sensor Data Availability

Presentation

The data transmitted by the environmental sensors to the Panel Server depends on the type of environmental sensor. The table indicates examples of data available in the Panel Server according to the type of environmental sensors.

Device Commercial References

The device commercial references used for each type of environmental sensor are:

  • CL110 (Contact your Schneider Electric representative for information about commercial references.)

  • TH110 (Contact your Schneider Electric representative for information about commercial references.)

  • TH150S, TH150M

  • TH200M

  • TRH (SED-TRH-G-5045)

  • TRHC02 (SED-CO2-G-5045)

For a full list of supported commercial references, refer to the following documents

  • DOCA0241EN EcoStruxure Panel Server - Modbus File

  • DOCA0249•• EcoStruxure Panel Server Entry - Firmware Release Notes

  • DOCA0178•• EcoStruxure Panel Server Universal - Firmware Release Notes

  • DOCA0248•• EcoStruxure Panel Server Advanced - Firmware Release Notes

Other Measurements

Data

CL110 TH110 TH150S TH150M TH200M TRH TRHC02

Temperature

Temperature phase A

Temperature phase B

Temperature phase C

Temperature neutral

Relative humidity

CO2 concentration

Internal temperature

Battery voltage

RSSI link

For a full list of measurements transmitted by environmental sensors, refer to DOCA0241EN EcoStruxure Panel Server - Modbus File.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.