DOCA0172EN-20

Modbus TCP/IP Server

Presentation

Devices connected downstream from the Panel Server can be accessed from an upstream edge system through Modbus TCP/IP.

Availability

This function is available on Panel Server Universal and Advanced.

Setting the Parameters

Modbus TCP/IP server function is set as follows:

  • With EcoStruxure Power Commission software

  • On the Panel Server webpages, at Settings > Modbus devices > Network configuration > Modbus TCP server.

Modbus TCP Server Settings

The following table describes the settings available from the webpages.

Parameter Description

Message timeout (ms)

In Modbus network configuration, you can set the message timeout period for the Modbus TCP server.

The setting is used to set the time-to-live of a Modbus request in the Panel Server. Any messages older than this setting will be dropped without sending any response back to upstream SCADA.

Enter a value from 1000 to 320000 ms with step 100 (default setting: 6000 ms).

The value that you set for the Modbus TCP server must meet both the following conditions:

  • Be equal to the message timeout that is defined on the upstream Modbus client (SCADA or another Panel Server).

  • Be higher than the timeout defined in the Panel Server Modbus client setting (Modbus TCP/IP and Modbus-SL).

For recommendations and more information about setting the parameter, refer to Setting Message Timeout for Modbus Client and Server.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.