DOCA0172EN-20

Removing Wireless Devices Through Webpages

Presentation

To remove one or several wireless devices through EcoStruxure Panel Server webpages, follow the procedures in the subsequent sections, as applicable:

  • Remove all connected wireless devices

  • Remove one connected wireless device

  • Forcing removal of one or several connected wireless devices

Some wireless devices have a local method to remove the devices. Refer to the instruction sheet of the specific device. For example, for wireless indication auxiliaries for ComPacT NSX and ComPacT NSXm circuit breakers, consult the instruction sheet available on the Schneider Electric website: NNZ8882801.

Procedure to Remove All Wireless Devices

  1. Navigate to Settings > Wireless devices > Network Configuration to view the list of discovered wireless devices.

  2. In the Wireless device management section, click the Remove all devices button.

    Result: A message displays to confirm the removal of the wireless devices from the configuration.

    NOTE: If your list of discovered wireless devices contains Exiway Link devices, a popup message is displayed to indicate that the removal of all devices may not function correctly. See Removing Exiway Link Devices for more information.
    NOTE: For removal of ZBRT devices, see Procedure to Remove a ZBRT Pushbutton Device.
  3. Click Yes to initiate the removal process for all devices in the Panel Server system.

  4. A progress bar shows the progress of the request execution. Wait until the progress bar is completed, indicating that all wireless devices should have received removal order. The process duration depends on the device. It may take up to 10 minutes.

    Result: Once a wireless device is successfully removed, it is no longer visible in the list of discovered wireless devices.

Procedure to Remove One Wireless Device

  1. Navigate to Settings > Wireless devices to view the list of discovered wireless devices.

  2. Select the device to be removed from the configuration.

  3. Click the bin icon on the right side of the webpage.

    NOTE: If the selected device is an Exiway Link device, a popup message is displayed to indicate that the removal of this device may impact other devices on the same network. See Removing Exiway Link Devices for more information.
    NOTE: For removal of ZBRT devices, see Procedure to Remove a ZBRT Pushbutton Device.
  4. Click Yes to initiate the removal process.

  5. Wait until removal is completed. The process duration depends on the devices. It may take up to 10 minutes.

    Result: Once the wireless device is successfully removed, it is no longer visible in the list of discovered wireless devices.

Procedure to Remove an XB5R Transmitter (ZBRT)

  1. In the webpages, navigate to Settings > Wireless devices to view the list of discovered wireless devices.

  2. Connect the ZBRZ1 commissioning module to the ZBRT pushbutton

    .
  3. Immediately press the ZBRT pushbutton six times to decommission the device.

  4. Wait 30 seconds.

    If the device in still on the discovered wireless devices list, continue with this procedure.

  5. Select the ZBRT pushbutton device to be removed from the configuration.

  6. Click the bin icon on the right side of the webpage.

  7. Click Yes to initiate the removal process.

    Result: The status of the device is shown as Removing.

  8. Click the Force remove button

NOTE: After performing a Remove all devices, the status of all connected ZBRT devices is shown as Removing. Perform a Force remove for each device individually.

Procedure to Force Removal of Wireless Devices

It is possible that the removal process of one or several devices is unsuccessful when a device is not powered or is out of order. If a device has not been removed 10 minutes after the removal process began, the status is shown as Removing in red in the list of discovered devices. You can force removal of a device from the Panel Server system.

To force device removal, from Settings > Wireless devices, select the device and click the Force remove button.

Result: Once the wireless device is successfully removed from the Panel Server configuration, it will not be visible in the list of discovered devices .

If you want to discover the forced removed device with a new Panel Server, reset and power off this device.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.