DOCA0172EN-20

User Management

Presentation

The default user account has administrator rights such as reading and changing the product configuration, adding or removing wireless devices, accessing system logs. The user account name of the user account is SecurityAdmin.

At first login, or after a factory reset, you must enter the default password: AAAAAAAA

You are then required to set a new user password. Comply with the password requirements.

Availability

This function is available on Panel Server Entry, Universal, and Advanced.

Changing the User Account Password

The user account password can be changed as follows:

  • With EcoStruxure Power Commission software

  • On any page of Panel Server webpages

    .
    1. Click the arrow next to the user account name in the header.

    2. Select Change password from the drop down list.

    3. Enter the old password.

    4. Enter the new password.

    5. Confirm the new password.

    6. Click Apply.

Password Requirements

The EcoStruxure Panel Server incorporates password requirements.

The user account password must conform to the following rules:

  • Must not be identical to the user account name

  • 8 to 50 characters

  • Must contain at least three of the following types of character:

    • Uppercase letters

    • Lowercase letters

    • Digits

    • Special characters limited to space character and !"#$%&'()*+,-./:;<=>?@[\]^_`{|}~

Password Lockout

After 10 invalid attempts to login to the EcoStruxure Panel Server, the user account is locked out.

When the user account is locked, the user must wait 10 minutes before being able to login again.

The user account is locked for 60 minutes each time there are 5 more invalid attempts.

User account lock state remains in case of reboot, including reboot after power loss.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.