DOCA0172EN-20

First Connection with EcoStruxure Power Commission Software

Presentation

EcoStruxure Power Commission software supports self-discovery of EcoStruxure Panel Server and connected devices.

Connection Procedure

Follow these steps to connect to the EcoStruxure Panel Server through EcoStruxure Power Commission

  1. Disconnect the PC from the local area network (LAN) and switch off Wi-Fi, if any.

  2. Connect an Ethernet cable from the PC to the Panel Server (see Connection to Ethernet).

  3. Open the EcoStruxure Power Commission application on your PC.

  4. Click the EcoStruxure Panel Server panel to launch self-discovery of the EcoStruxure Panel Server.

  5. Identify your EcoStruxure Panel Server by selecting the correct MAC address (see the MAC address on the top of your EcoStruxure Panel Server).

  6. Click Next to open the device page.

  7. Click Add device.

  8. When the EcoStruxure Panel Server displays with the device characteristics, click the green Connect button.

    During the connection, a firmware update is proposed. Follow the on-screen instructions to update the firmware. Click the cross at the top right of the window to come back to the device page.

  9. When the connection is complete, start the commissioning of the EcoStruxure Panel Server.

If the self-discovery does not find the Panel Server, refer to Troubleshooting.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.