DOCA0172EN-20

Discovery of XB5R Transmitters (ZBRT)

Presentation

XB5R transmitters for wireless and batteryless ZBRT pushbutton devices can be discovered in the Panel Server.

Discovery Procedure

  1. Launch the Panel Server webpage in the web browser.

  2. Log in to the webpages (see how to access the webpages).

  3. Navigate to Settings > Wireless devices > Discovery and click Automatic.

  4. Check that the ZBRZ1 commissioning module is not connected to any ZBRT pushbutton device.

  5. Click Start.

  6. Connect the ZBRZ1 commissioning module to each ZBRT pushbutton device in turn. For more information, consult the ZBRZ1 Instruction sheet NNZ21729.

  7. Maintain the connection for a few seconds. The ZBRT device is paired when the accessory is connected, and appears in the discovery result table.

  8. Once discovery is completed you can view the list of the discovered wireless devices in webpage Settings > Wireless devices > Wireless devices.

  9. Configure the wireless devices.

    NOTE: The Modbus virtual ID assigned to the wireless devices can be changed after the discovery process is done.

Configuration Procedure

To configure ZBRT devices with Panel Server webpages, proceed as follows:

  1. Navigate to Settings > Wireless Devices to view the list of the discovered wireless devices.

    Result: The list of discovered devices is displayed (with Connected written in green under the device name).

  2. Select the required device to modify its configuration.

    Result: The parameters of the device are displayed.

  3. Enter the data in the fields, referring to the following tables for more information about the parameters.

  4. Save your settings by clicking the icon at the bottom right of your screen and selecting Save.

Parameter Tables

Identification

Parameter name Description

Name

Enter the name of the wireless device.

Label (optional)

Enter the label of the wireless device.

Device range

For display only

Commercial reference

For display only

Hardware revision

For display only

Device family

For display only

Modbus virtual

Parameter name Description

Virtual server ID

Enter the ID of the Modbus virtual server.

Contextualization data

Parameter name Description

Commodity (optional)

Select the commodity required from the list to indicate the main purpose of the device.

Usage (optional)

Select the usage required from the list to indicate the precise function of the device.

Zone (optional)

Select the zone in the list, as contextualization data.

Click the Settings icon to:

  • Create a new zone

  • Modify a zone name

  • Delete a zone

For more information about creating, modifying and deleting zones, refer to Zone Management.

Setting the Retention Time for ZBRT1 Pushbutton Devices

The retention time is the length of time the ZBRT1 pushbutton status remains ON after being pressed.

Set the button status retention time of the ZBRT1 pushbutton device between 100 and 1000 ms (default value 500 ms) at Settings > Wireless devices > Global functional settings. Select a value from the list.

Removal Procedure

Follow the removal procedure for ZBRT devices, described in Removing Wireless Devices Through Webpages.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.