DOCA0172EN-19

EcoStruxure Panel Server Modbus Registers

The Panel Server implements its own Modbus registers which start at address 255.

For a full list of available data, refer to DOCA0241EN EcoStruxure Panel Server - Modbus File.

The available data includes the following settings:

  • Modbus TCP/IP server settings:

    • Modbus ID of Panel Server

    • Message timeout: (Modbus TCP/IP server)

  • Modbus TCP/IP client settings:

    • Timeout of Modbus TCP/IP client

    • Message timeout of Modbus TCP/IP client request

  • Modbus SL settings for downstream communication:

    • Modbus parity

    • Modbus baud rate

    • Number of stop bits

    • Silent interval after Modbus SL packet end

    • Delay between Modbus SL packets

    • Connect/Disconnect the RS485 termination resistor

    • Transmission line state

  • Modbus SL client settings

    • Message timeout of Modbus SL request

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?