DOCA0172EN-20

Configuration of Wireless Indication Auxiliaries

Presentation

Wireless indication auxiliaries can be configured through Panel Server webpages.

Configuration Procedure

To configure wireless indication auxiliaries, follow the procedure in Configuring Wireless Devices Through Webpages.

The following tables list the parameters for the configuration of wireless indication auxiliaries.

Parameter Tables

Identification

Refer to Configuring Wireless Devices Through Webpages.

Communication Settings

Parameter name Description

Communication period

8 hours (for display only)

Modbus virtual

Refer to Configuring Wireless Devices Through Webpages.

Auxiliary position

Parameter name Description

Auxiliary position

Select the position from the list.

Contextualization data

Refer to Configuring Wireless Devices Through Webpages.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?