DOCA0172EN-20

EcoStruxure Power Commission Web Tool (EPC Web)

Overview

The EcoStruxure Power Commission Web tool is intended to help system integrators save time to execute their projects by offering the following actions so that you can cater to different customer requirements in terms of events or measurements of devices to be monitored:

  • Giving access to a common single device model library that can be used on any EcoStruxure Panel Server.

  • Giving you the ability to manage your own device models by creating, testing, and deploying them.

  • Giving access to cloud connected gateways and devices to associate required models.

A custom device model in the EcoStruxure Power Commission Web tool contains the list of measurements, alarms, Modbus frames and events that can be used to monitor Modbus based devices in the field. The user can create, edit, view, and export device model data as per the requirement.

Key Features

The EcoStruxure Power Commission Web tool allows you to perform the following actions:

  • Create a model: Create from scratch reusable device models for monitoring Modbus devices using EcoStruxure Panel Server.

  • View and Export Models: Select and export device models previously created by you or others so that they can be imported in EcoStruxure Panel Server.

Detailed help and instructions for creating a device model are available in the EcoStruxure Power Commission Web tool at Help > Documentation.

For more information, go to EcoStruxure Power Commission Web.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.