First Connection with EcoStruxure Power Commission Software
Presentation
EcoStruxure Power Commission software supports self-discovery of EcoStruxure Panel Server and connected devices.
Connection Procedure
Follow these steps to connect to the EcoStruxure Panel Server through EcoStruxure Power Commission
-
Disconnect the PC from the local area network (LAN) and switch off Wi-Fi, if any.
-
Connect an Ethernet cable from the PC to the Panel Server (see Connection to Ethernet).
-
Open the EcoStruxure Power Commission application on your PC.
-
Click the EcoStruxure Panel Server panel to launch self-discovery of the EcoStruxure Panel Server.
-
Identify your EcoStruxure Panel Server by selecting the correct MAC address (see the MAC address on the top of your EcoStruxure Panel Server).
-
Click Next to open the device page.
-
Click Add device.
-
When the EcoStruxure Panel Server displays with the device characteristics, click the green Connect button.
During the connection, a firmware update is proposed. Follow the on-screen instructions to update the firmware. Click the cross at the top right of the window to come back to the device page.
-
When the connection is complete, start the commissioning of the EcoStruxure Panel Server
If the self-discovery does not find the Panel Server, refer to Troubleshooting.