DOCA0172EN-15

Getting Started with EcoStruxure Panel Server Webpages

Follow these stages to set up the Panel Server device through the webpages:

  1. Connect the Panel Server. Refer to First Connection to Panel Server Webpages.

  2. Set the date and time for the Panel Server at Settings > General. Refer to Date and Time.

  3. Configure the network settings.

  4. Add Modbus devices and/or discover wireless devices.

  5. Configure the connected devices:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?