DOCA0172EN-15

Permanent Deactivation of Wireless Networks

Presentation

Panel Server models PAS600LWD and PAS600PWD natively have no IEEE 802.15.4 or Wi-Fi wireless network capability.

IEEE 802.15.4 and Wi-Fi wireless networks can be permanently and concurrently disabled in other Panel Server Universal models and in Advanced models. Once the wireless networks are disabled via this command, it is permanent and cannot be undone. Neither a factory reset, nor a backup restore can activate the radio capabilities again. If an IEEE 802.15.4 or Wi-Fi network is required, the Panel Server must be replaced by a new one.

The permanent deactivation of the wireless networks is not saved in the backup file of Panel Server configuration (see detailed topic).

Availability

This function is available on Panel Server Universal (except WD models, which have no wireless capability) and Panel Server Advanced.

Setting the Parameters

Permanent deactivation of wireless networks is set on the EcoStruxure Panel Server webpages, at Settings > Security > Network Management > Wireless networks disable.

Deactivating Wireless Networks Permanently

NOTICE
Permanent loss of communication with wireless devices
Permanent deactivation of wireless networks permanently disables communication with wireless devices. Only follow this procedure if you are sure you do not want to communicate with wireless devices in the future.
Failure to follow these instructions can result in unintentional loss of communication.

To permanently and concurrently disable the IEEE 802.15.4 and Wi-Fi wireless networks in the Panel Server, proceed as follows:

  1. In the Network Management webpage, click Disable all wireless networks.

  2. Read the pop-up message carefully before confirming or cancelling the deactivation in the window that appears.

    Result: After confirming deactivation, the Panel Server automatically reboots. After rebooting, both types of wireless network are permanently deactivated in the Panel Server and indicated as such on the webpages. The deactivation is irreversible.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?