NHA2779005-11

Cumplimiento de normas aplicables en China

Este producto cumple la(s) siguiente(s) norma(s) aplicable(s) en China:

PM2110 / PM2120

BS/ EN/ IEC/ UL 61010-1 Safety requirements for electrical equipment for measurement, control, and laboratory use - Part 1: General requirements

PM2130

BS/ EN/ IEC 61557-12 Electrical safety in low voltage distribution systems up to 1 000 V AC and 1 500 V DC - Equipment for testing, measuring or monitoring of protective measures - Part 12: Power metering and monitoring devices (PMD)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

¿Le ha resultado útil?