Change CU
- In the Project pane, find the line item where you want to add the install CU.
-
Hover over the options
icon for that item, then click the Change CU
tool.
-
After the CU Search appears, type in the CU name or attributes
to find the appropriate CU. Once found, double-click it to accept
the changes.
TIP:
-
You can also change the CU using the right-click context wheel.
-
You can use the Change CU tool for any work function.
-
You can use the Change CU tool to change the load on a service point. If using the right-click context wheel on a service point, the tool is called “Change Load” instead of “Change CU.”
-