Inspect

The Inspect tool displays attributes of features in a Reference view.


To use this tool:

  1. Toggle the Reference view that contains your desired features on . This tool does not work if the Reference view is off.

  2. Click the Inspect tool.

  3. In the map, click the feature and view its attributes in the pop up. This tool works with points, lines, and polygons (shapes with an area).

    IMPORTANT: This tool only works with features within the Reference view. To see attributes of network components in or near your design, use the Component Information pane.

  4. Press Esc when finished viewing the attributes.


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?