Fuse

A fuse is a protective device with single or multiple phases.

Sketching

  • Fuses snap to conductors and inherit the conductor’s phasing. If sketching a single-phase fuse onto a multiple-phase conductor, you are prompted to choose the appropriate phase once sketched.

  • A fuse will split an existing conductor into two sections.

  • Once sketched, the device can be operated (open or closed) by phase in the Component Information pane.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?