Print Pages Pane

Much like the Design tab and the Project pane work together, the Print tab and the Print Pages pane work together. After creating a print layout using the Print tab, the Print Pages pane facilitates multi-page printing. It allows you to create additional pages, re-order pages, and re-name pages as part of a larger print book.

For more information, please see the Print Tab and Print Multiple Pages topics.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?