Component Information Pane

The Component Information pane provides detailed information about any components you have selected. This pane can be used with components that were initialized in the design from the GIS or with components you have placed in your design.

Each type of feature you select has slightly different pieces of information available to view, and in some cases, interact with across the application. In general, you have a Facility ID, component information, associated CUs, and if the device is operable, an open or closed toggle.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?