Print Tab
Modifying or creating the printed map to be included in your construction packet can easily be accomplished on the Print Tab.
This tab contains all tools related to finishing out the project with a presentable map.
Using a Pre-Defined Print Template
One of the most helpful time-savers on the Print tab is to employ a pre-defined print template. These are created by an administrator (with user input, of course) and shared across the organization. A well-defined template can accomplish almost all the printable tasks for you.
On the Print Pages pane, click the Add
icon.
Then, choose a template. Templates are sorted ascending by name (the names in the image below are examples and differ from your company’s templates).
After applying the template, you can make further modifications to the print.
The subsequent help topics discuss these modifications including extent, navigation, and adding print elements.
Print Progress Bar
After you send the map to the printer (or to PDF), a progress bar appears:
While the application is generating the print map, the interface locks and most functions are disabled until the print is complete.