Refresh Layers

Click Refresh Layers to get the most up to date features included in the Reference maps.

When you open a design, the features in the Reference maps are cached and are therefore static. However, new features might have been added to a feature service since the time you opened your design. This is particularly true with a service such as Work Areas, where other designers might be working in your design vicinity. Click Refresh Layers for the application to grab the most up to date features and display them on your map.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?