Measure Tool
The Measure Tool sketches linear measurements on the map, complete with segment lengths, angles of deflection, and total length.
-
Measurement lines are saved with your design, but they are not pushed back to the GIS.
-
They provide helpful reference lengths and angles that can guide your design process.
-
The size of the length and angle labels is not configurable. It is controlled by the application.
-
You can increase or decrease the Reference Scale to change the size of the labels, but keep in mind, that affects all labels and elements on the map. See the topic Design Style for more information about the Reference Scale.
-
To Sketch a Linear Measurement:
-
Bring your cursor into the map.
-
Click once to start your measurement.
-
Each subsequent click adds a vertex (or bend) in the line. Segment lengths are displayed at each segment, angles of deflection are displayed at each vertex, and the current total length is displayed near your cursor.
TIP: To cancel mid-sketch, press Esc. -
Double-click to finish the measurement sketch.
-
When the measurement sketch is finished, it persists on the map. Notice, a tool tip informs you that you can discard the most recent measurement by clicking the middle mouse button.
TIP: Don’t have a middle mouse button? Press Backspace.
To Delete a Linear Measurement: