Custom Properties for the Design

Custom Properties allow you to save high-level properties for the Design itself. These properties are sent along with your design through the workflow, and they can even integrate with your company’s Work Management System (WMS).

You can find the available properties directly beneath the Design Notes (Custom Properties vary by company, so the fields in the image below likely differ from your available fields).

TIP: If you are an administrator, you can configure Custom Properties in Solution Center > Designer > Client Application > Backstage Custom Properties.

After populating the Custom Properties, click Save.

TIP: Did you receive an error notification after clicking Save? Look for which field is outlined in red. The most common issue is a data type mismatch, for example, typing text when the field is expecting a date.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?