Print Tab

The Print tab is the interface for creating the maps and documentation needed to share your designs with others.

It allows for different map views, labels, and text block configurations to display what you want and where you want it. Rich text formatting allows for a variety of colors and styles. Administrators can also create templates to support quick and easy mapping and printing.

By default, the tab is “locked” in a position where it is visible at all times. Double-click the tab to enable auto-hide, where the tab collapses while you interact with the map or other panes. To return to the locked position, double-click the tab again.

When you click the Print tab, your design is displayed within the first template in the predefined print templates menu. Adjust the map view as needed so that the appropriate content is displayed, update any text boxes as needed, save, then print.

More detailed information about this tab is in the detailed Print tab topic.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?