Map Space Management

There are a variety of tools that help you clean up the design area, which is especially useful for printable maps. These tools include:

  • Hide Label and Show Label

  • Move Label and Change Label Style

  • Hide Component

    • Discover Tool (reveals previously hidden component)

  • Map Clipper

All the tools above, except for Map Clipper, can be used in both the Design tab and Print tab.

Each tool has a subsequent help topic in this chapter.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?