Span Guy

A span guy is a linear feature providing support for one or multiple poles.

Sketching

  • Click in the map to place a new span guy. Sketching a span guy is a two-click process, and intermediary vertices are not allowed in the initial sketch.

    • After you sketch a span guy, you can right-click it and choose Move. Then, you can add more vertices. See Move Install CUs and Work Locations for more information about modifying linear features.

  • Span guys snap to poles.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?