Component Search Pane

The Component Search allows you to search for components that were imported into the design, in addition to components that you have placed as part of your design.

On the left-hand side of the interface, click the Component Search button to open the search pane.

To search for a component, start typing in the field. Once you type three characters/numbers, the search automatically starts returning results. As you type more, the list gets filtered down automatically.

The search is looking at all component types and is searching on the Facility ID field. The results are grouped together by component type and are listed in alphanumeric order.

Once you find what you are seeking, you can click that component. It becomes selected and the map zooms to that location.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?