Copy WL CU Text

The Work Location is a logical grouping point for CUs.

To extract all the CU information at a particular Work Location, follow these steps:

  1. In the Project pane, hover over the Work Location, then click Copy WL CU Text.

  2. Paste the text as needed, for example, in a Map Note for printing purposes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?